Disassembling Clamp Connection

Clamp disassembly

  1. Remove the screws in the blue lid, then remove the blue lid, as shown in section General Guidance to Separate Joint from Counterpart.
  2. Gently remove the power and communications wires from the terminals, as shown in section Power and Communication Connector Types on the Joint and Connector Location on joints.
  3. Remove the black flat ring. You can use a small flat-head screwdriver.

 
  1. Remove the screws and the clamp on one side.
The joint can fall off if not supported when removing the clamp.

  1. Support the joint as you remove the second side of the clamp.



  1. The joint is now loose and can be removed. Remember to pull the wires out as well.