Disassembling Screw Connection
-
Remove the screws in the blue lid, then remove the blue lid as shown in Section General Guidance to Separate Joint from Counterpart
-
Gently remove the power and communications wires from the terminals as shown in Section Power and Communication Connector Types on the Joint and Connector Location on joints.
- You can use a small flathead screwdriver to push-off the flat-ring.
Then slide the flat-ring over the joint. - Remove Teflon-ring.
The joint can fall off if not supported when removing the screws.
-
First remove the countersunk screws(a) then the remaining(b) screws.
Note: Be very careful when removing the screws. Always use a correct sized, and undamaged screwdriver. The screw head slots can easily be stripped.
-
The joint is now loose and can be removed. Remember to pull the wires out.