Accessing System and Security
Description |
The Admin password is also required to access System and Security, see Administrator Password. When you change the default password to your own password, you can use it to access the settings under System (see System ) and to access the settings under Security (see Security ). The default admin password for a Universal Robots robot arm controller is “easybot”. It is a factory setting, configured on all new robots. It is critically important that you change this default admin password to your own password, to ensure cyber security of your robot. As of PolyScope update 5.17 all security settings are set by default to restrictive (disabled or blocked). (This only applies to new robots and newly created SD-cards. Otherwise, refer to a guide “Secure setup of UR cobots”). If any of the settings are needed to be enabled for your application, you can easily enable them in the Security screen.
|
To use the Admin password |
|