Administrator Password

Description

Use the Administrator (Admin) Password to change the security configuration of the system, including network access.

The Admin password is equal to the password used for the root user account on the Linux system running on the robot, which may be needed in some network use cases such as SSH or SFTP.

You cannot recover a lost Admin password.

  • Take the appropriate steps to ensure your admin password is not lost.

 

To set the Admin Password
  1. In the Header, tap the Hamburger menu icon and select Settings.

  2. Under Password, tap Admin.

  3. Under Current password, put in the default password: easybot.

  4. Under New password, create a new password.

    Creating a strong, secret password obtains the best security for your system.

  5. Under Confirm new password, repeat your new password.

  6. Tap Apply to confirm your password change.

Safety

The Safety password prevents unauthorized modification of the Safety settings.