Software installation

This section describes how to configure the IMMI module software. For information on installing the IMMI module hardware, see Hardware installation.

Configuring the IMMI module software

To configure the IMMI module software

  1. On PolyScope, in the Header, tap Installation and select Safety.

  2. Tap Hardware and unlock the options on the Select available hardware screen.

    A password is required to unlock this screen.

  3. In the Injection molding machine interface drop-down list, select the desired recommendation.

  4. Tap Apply to restart the system. PolyScope continues to run.

  5. Tap Confirm Safety Configuration to complete the IMMI software installation.

Uninstalling the IMMI module

To uninstall the IMMI module

  1. On PolyScope, use your password to access the Select available hardware screen.

  2. In the Injection molding machine interface drop-down list, select None.

  3. Tap Apply to restart the system. PolyScope continues to run.

  4. Tap Confirm Safety Configuration.

  5. Power down the control box and disconnect the mains cable from the power source.

  6. Disconnect the IMM plug from the IMMI module.

  7. Dismount the interface.

    • Remove the ribbon cable.
    • Remove the M6 nut to disconnect ground connector.
    • Remove the M6 screws and tooth lock washers to remove the IMMI module.
    • Use the M6 screws and tooth lock washers to reattach the plate to the control box.