|
When performing the application risk assessment, it is necessary to take into account the motion of the robot after a stop has been initiated. In order to ease this process, the safety functions Stopping Time Limit and Stopping Distance Limit can be used.
These safety functions dynamically reduce the speed of the robot motion such that it can always be stopped within the limits.
The joint position limits, the safety planes and the tool/end effector orientation limits take the expected stopping distance into account, i.e., the robot motion will slow down before the limit is reached.
|