example: tool_contact
Example of usage in conjunction with the "get_actual_joint_positions_history()" function to allow the robot to retract to the initial point of contact:
>>> def testToolContact():
>>> while True:
>>> step_back = tool_contact()
>>> if step_back <= 0:
>>> # Continue moving with 100mm/s
>>> speedl([0,0,-0.100,0,0,0], 0.5, t=get_steptime())
>>> else:
>>> # Contact detected!
>>> # Get q for when the contact was first seen
>>> q = get_actual_joint_positions_history(step_back)
>>> # Stop the movement
>>> stopl(3)
>>> # Move to the initial contact point
>>> movel(q)
>>> break
>>> end
>>> end
>>> end
Example command: tool_contact(direction =
get_target_tcp_speed())
- Example Parameters:
- direction=get_target_tcp_speed() will detect contacts in the direction of TCP movement
tool_contact(direction = [1,0,0,0,0,0])
- Example Parameters:
- direction=[1,0,0,0,0,0] will detect contacts in the direction robot base X