get_actual_tcp_pose()
Returns the current measured tool pose
Returns the 6d pose representing the tool position and orientation specified in the base frame. The calculation of this pose is based on the actual robot encoder readings. See details about pose representation in Numbers, Variables, and Types
Return Value
The current actual TCP vector [X, Y, Z, Rx, Ry, Rz]