Visual Inspection: Robot Arm

 

Using compressed air to clean the robot arm can damage the robot arm components.

  • Never use compressed air to clean the robot arm.
 

You can see the torque values and other technical data used to adjust the robot after the visual inspections here: Connection Torque Values

 

  1. Move the Robot Arm to ZERO position, if possible.
  2. Turn off and disconnect the power cable from Control Box.
  3. Inspect the cable between Control Box and Robot Arm for any damage.
  4. Check the base mounting bolts are properly tightened.
  5. Check the tool flange bolts are properly tightened.
  6. Inspect the flat rings for wear and damage.
    • Replace the flat rings if they are worn out or damaged.
If any damage is observed on a robot within the warranty period, contact the distributor where the robot was purchased.