Preventive Measures
| Preventive Measures |
Ignoring Robot stops is considered abuse of the robot which voids the warranty. These faults can be hidden from view under the following two circumstances:
Ignoring robot stops masks fault detection, which can increase the risk of injury.
Robot stops must never be acknowledged and reset automatically, it must always be a deliberate action by a user to resume after a robot stop. In general, robot stops are designed to inform the user that the robot has stopped due to an external event such as hitting an obstacle or similar. In case the robots are pushed close to the limits, the robots can generate robot stops to indicate that they are not capable of following the desired trajectory. After a robot stop, the following must be done before resuming operation:
Robot stops are indications of issues, including program or production issues – not only safety issues. An application which results in daily robot stops is not designed correctly and needs to be modified.
Automatic acknowledgment and reset of robot stops masks faults that will lead to a failure condition.
If an integrator has set-up the application program to do automatic acknowledgement and reset of robot stops, the customer should contact the integrator change the program immediately, as such override voids the product warranty and masks fault detection.
|