Cybersecurity Hardening Guidelines

 

Description

Although PolyScope includes many features for keeping the network connection secure, you can harden security by observing to following guidelines:

  • Before connecting your robot to any network, always change the default password to a strong password.

  • You cannot retrieve or reset a forgotten or lost password.

    • Store all passwords securely.

  • Use the built-in settings to restrict the network access to the robot as much as possible.

  • Some communication interfaces have no method of authenticating and encrypting communication. This is a security risk. Consider appropriate mitigating measures, based on your cybersecurity threat assessment.

  • SSH tunneling (Local port forwarding) must be used to access robot interfaces from other devices if the connection crosses the trust zone boundary.

  • Remove sensitive data from the robot before it is decommissioned. Pay particular attention to the URCaps and data in the program folder.

    • To ensure secure removal of highly sensitive data, securely wipe or destroy the SD card.