General Cybersecurity

Description

Connecting a Universal Robots robot to a network can introduce cybersecurity risks.

These risks can be mitigated by using qualified personnel and implementing specific

measures for protecting the robot's cybersecurity.

Implementing cybersecurity measures requires conducting a cybersecurity threat assessment.

The purpose is to:

  • Identify threats

  • Define trust zones and conduits

  • Specify the requirements of each component in the application

Failure to conduct a cybersecurity risk assessment can place the robot at risk.
  • The integrator or competent, qualified personnel shall conduct a cybersecurity risk assessment.
Only competent, qualified personnel shall be responsible for determining the need for specific cybersecurity measures and for providing the required cybersecurity measures.