UR Connect

Connect PolyScope X to myUR Cloud

You have to connect your PolyScope X software to the myUR Cloud service.

You need to find you PIN code in your myUR account.

  1. Go to Settings.

  2. Go to UR Connect.

  3. Hit the "Connect" button on the main UR Connect page.

  4. Add you pin code from myUR.

When you see the green icon in the right corner of the window, you are connected to the myUR Cloud.

Unsuccessful connect

If you see the "Incorrect PIN code", please review your PIN code from myUR.

 

Diagnostics

If you experience any unexpected when the UR Connect is active, you can go to the Diagnostics.

  1. Go to Settings.

  2. Go to UR Connect.

  3. Hit the kebab menu in the top right corner.

  4. Select the "Diagnostics".

 

Export logs

It is possible to export the UR Connect logs from your PolyScope X software.

  1. Go to Settings.

  2. Go to UR Connect.

  3. Hit the kebab menu in the top right corner.

  4. Select the "Export Logs"

  5. Select "Export to myUR" or "Export to USB".