Automatic Mode Safeguard Stop
| Description |
Automatic Mode Safeguard Stop is a new configurable safety input with accompanying reset. When enabled, it performs a safeguard stop when the input pins are low and the robot is in automatic mode. This input has no effect in the manual mode. When Automatic Mode Safeguard Stop is activated, the robot must do a category 2 stop, which means that the robot stops, but power is still allowed on the motors.
|
| Details |
Similar to the Safeguard Reset, if you disable the default Automatic Mode Safeguard Reset, the robot arm is no longer Safeguard Stop stopped once the Automatic Mode Safeguard Stop input is high. A program paused only by the Automatic Mode Safeguard Stop resumes.
Automatic Mode Safeguard Stop is a condition that activates a robot’s Safeguard Stop:
|
|
Access Automatic Mode Safeguard Stop |
|
|