Set

Description

The Set command enables you to set a given value to either digital or analog outputs.

 

To access Set command

  1. Go to the main program screen. See Command Nodes.

  2. Tap the Set icon in the Commands toolbox.

  3. A node with an editable Source field is inserted into the program tree that enables you to select Wired IO and Tool IO.

  4. Tap the Source field.

     
 
  1. When you select Wired IO, a Signal field is inserted.

  2. In the Signal field, tap your preferred signal.

    • DO 0–DO 7: Digital signal

    • CO 0–CO 7: Digital signal

    • AO 0–AO 1: Analog signal

  3. When a digital signal is selected, a Value field is inserted to the right.

  4. Choose either High or Low.

  5. When an analog signal is selected, a Value field is inserted to the right.

  6. Enter data in the Value, Variable, and Expression tabs, and tap Confirm. See Value-Variable-Expression Tabs.

  7. When you select Tool IO, a Signal field is inserted.

  8. Choose either DO 0 or DO 1.

    A Value field is inserted to the right with three options:

    • Use Variable

    • High

    • Low

  9. Tap Use Variable, and the Variable and Expression tabs appear.

  10. Enter data in the two tabs, and tap Confirm. See Value-Variable-Expression Tabs.

  11. You can also choose either High or Low in the Value field.