set_tool_analog_input_domain(port, domain)

Set domain of analog inputs in the tool

For the controller box inputs see set_standard_analog_input_domain.

Parameters

port: analog input port number: 0 or 1

domain: analog input domains: 0: 4-20mA, 1: 0-10V

Example command: set_tool_analog_input_domain(1,1)

  • Example Parameters:
    • port = tool analog input 1
    • domain = 1 (0-10 volts)