public interface SystemConfiguration
| Modifier and Type | Method and Description |
|---|---|
CapabilityManager |
getCapabilityManager()
Access an interface that can be used for verifying that specific capabilities are available on the underlying
robot/system.
|
ControllableResourceModel |
getControllableResourceModel()
Access an interface for requesting exclusive control of system resources, e.g.
|
ResourceModel |
getResourceModel() |
CapabilityManager getCapabilityManager()
RequiredCapability.ResourceModel getResourceModel()
ControllableResourceModel getControllableResourceModel()
Access an interface for requesting exclusive control of system resources, e.g. the Tool I/O interface.
NOTE: Requesting control of a system resource must happen in the scope of theGripperContribution.configureInstallation(CustomUserInputConfiguration, SystemConfiguration, TCPConfiguration, GripperAPIProvider)
method.Copyright © 2019. All rights reserved.