| Interface | Description |
|---|---|
| AnalogInputUntilNodeConfig | |
| BlendParameters | |
| CustomBlendParameters | |
| CustomDecelerationParameters | |
| DecelerationParameters | |
| DigitalInputUntilNodeConfig | |
| DistanceUntilNodeConfig | |
| ExpressionUntilNodeConfig | |
| FloatRegisterInputUntilNodeConfig | |
| IOInputUntilNodeConfig | |
| ReachedWaypointUntilNodeConfig | |
| UntilNodeConfig |
This interface represents a configuration of the Until program node.
|
| UntilNodeConfigFactory |
This interface can be used to create configurations that can be applied to an Until program node.
|
| Enum | Description |
|---|---|
| AnalogInputUntilNodeConfig.InputDomainType |
The type of the electrical domain used by an analog input.
|
| BlendParameters.ParameterType |
Blend Parameters can be of different types
The parameter type is used to determine the explicit blend parameters (can be used in place of instanceof operations)
|
| CustomDecelerationParameters.Type | |
| DecelerationParameters.ParameterType |
The deceleration parameter type used to determine which type of deceleration parameter this instance is.
|
| IOInputUntilNodeConfig.SelectionType |
The type of the input selection
|
| UntilNodeConfig.ConfigType |
The configuration type used to determine which type of configuration this instance is.
|
Copyright © 2019. All rights reserved.