public interface WaitNode extends ProgramNode
| Modifier and Type | Method and Description |
|---|---|
WaitNodeConfig |
getConfig() |
WaitNodeConfigFactory |
getConfigFactory() |
WaitNode |
setConfig(WaitNodeConfig config)
Set a configuration on this node.
|
WaitNodeConfigFactory getConfigFactory()
WaitNode setConfig(WaitNodeConfig config)
config - the configuration to be set.InvalidDomainException - if config is analog input using voltage and the IO is configured to current
or vice versa.IllegalStateException - if called from a Swing-based URCap outside of an UndoableChanges scope (see also UndoRedoManager)WaitNodeConfig getConfig()
Copyright © 2019. All rights reserved.