public interface Mass
This interface represents mass values.
The mass values can be created using theSimpleValueFactory interface.| Modifier and Type | Interface and Description |
|---|---|
static class |
Mass.Unit |
| Modifier and Type | Method and Description |
|---|---|
boolean |
equals(Object obj)
Indicates whether some other
Mass object is "equal to" this one. |
double |
getAs(Mass.Unit unit)
Provides the value in specified units.
|
int |
hashCode() |
String |
toString() |
Copyright © 2024. All rights reserved.