| Interface | Description |
|---|---|
| AnalogInput | |
| AnalogInputCurrentWaitNodeConfig | |
| AnalogInputSelection | |
| AnalogInputVoltageWaitNodeConfig | |
| AnalogInputWaitNodeConfig | |
| DigitalInput | |
| DigitalInputSelection | |
| DigitalInputWaitNodeConfig | |
| ExpressionInputWaitNodeConfig | |
| FloatRegisterInput | |
| FloatRegisterInputSelection | |
| FloatRegisterInputWaitNodeConfig | |
| TimeWaitNodeConfig | |
| WaitNodeConfig | |
| WaitNodeConfigFactory |
The WaitNodeConfigFactory can be used to construct configurations that can be set on a WaitNode.
|
| Enum | Description |
|---|---|
| AnalogInputSelection.SelectionType | |
| DigitalInputSelection.SelectionType | |
| FloatRegisterInputSelection.SelectionType | |
| WaitNodeConfig.ConfigType |
The configuration type used to determine which type of configuration this instance is.
|
Copyright © 2024. All rights reserved.