public interface AnalogInputUntilNodeConfig extends IOInputUntilNodeConfig
| Modifier and Type | Interface and Description |
|---|---|
static class |
AnalogInputUntilNodeConfig.InputDomainType
The type of the electrical domain used by an analog input.
|
IOInputUntilNodeConfig.SelectionTypeUntilNodeConfig.ConfigType| Modifier and Type | Method and Description |
|---|---|
CompareOperator |
getCompareOperator() |
Current |
getCurrentThreshold() |
AnalogIO |
getInput()
Retrieves the selected analog input used by the until condition.
|
AnalogInputUntilNodeConfig.InputDomainType |
getInputDomainType() |
Voltage |
getVoltageThreshold() |
getTypegetConfigTypeAnalogInputUntilNodeConfig.InputDomainType getInputDomainType()
AnalogIO getInput()
Retrieves the selected analog input used by the until condition.
Note: The selected analog input might no longer be available (e.g. because a selected analog Tool input is used for Tool Communication Interface). The presence of the selected analog input can be verified usingAnalogIO.isResolvable().CompareOperator getCompareOperator()
Current getCurrentThreshold()
IllegalStateException - if the selected analog input is using the Voltage electrical domain. Use
getInputDomainType() to determine the electrical domain type used by the selected analog input.Voltage getVoltageThreshold()
IllegalStateException - if the selected analog input is using the Current electrical domain. Use
getInputDomainType() to determine the electrical domain type used by the selected analog input.Copyright © 2024. All rights reserved.