| Interface | Description |
|---|---|
| CustomParametersPayloadNodeConfig |
This interface represents a configuration of the Set Payload node which is using custom payload parameters.
|
| PayloadNodeConfig |
This base interface represents a configuration of the Set Payload program node, i.e.
|
| PayloadNodeConfigFactory |
This interface can be used to create configurations that can be applied to a Set Payload program node, i.e.
|
| SelectionPayloadNodeConfig |
This interface represents a configuration of the Set Payload node where a payload (from the installation) has been
selected.
|
| Enum | Description |
|---|---|
| PayloadNodeConfig.ConfigType |
The configuration type used to determine which type of configuration this instance is.
|
Copyright © 2024. All rights reserved.