| Class and Description |
|---|
| LoopNodeConfig |
| LoopNodeConfigFactory
This interface can be used to construct configurations that can be set on a Loop program node.
|
| Class and Description |
|---|
| AlwaysLoopNodeConfig |
| CounterLoopNodeConfig |
| ExpressionLoopNodeConfig |
| LoopNodeConfig |
| LoopNodeConfig.ConfigType
The configuration type used to determine which type of configuration this instance is.
|
Copyright © 2024. All rights reserved.