| Interface | Description |
|---|---|
| ScrewdriverProgramList |
This interface represents the list of programs, typically defined on an external control box for the screwdriver.
|
| ScrewdriverProgramListProvider |
This interface must be implemented by the screwdriver URCap to register the program selection capability.
|
| Class | Description |
|---|---|
| ScrewdriverProgram |
This abstract class represents a screwdriver program, typically defined on an external control box for the screwdriver.
|
| Exception | Description |
|---|---|
| DuplicateScrewdriverProgramID |
This exception is thrown when the provided list of screwdriver programs (see
ScrewdriverProgramList) do not
have a unique identifier for all programs. |
| NameOfScrewdriverProgramCannotBeNullOrEmpty |
This exception is thrown when an attempt is made to add a screwdriver program (using the
ScrewdriverProgramList interface) without a proper display name, i.e. |
Copyright © 2024. All rights reserved.