public interface GripperListProvider
This interface must be implemented by the gripper URCap to register the multi-gripper capability. The implementation is responsible for providing PolyScope the list of individual grippers/zones available in the multi-gripper device.
Pass the implementation of this interface to the GripperCapabilities.registerMultiGripperCapability(GripperListProvider)
method when registering the multi-gripper capability.
getGripperList(GripperListBuilder, Locale) is only called once when the capability is registered, so
it is not possible to add more grippers at later time.| Modifier and Type | Method and Description |
|---|---|
GripperList |
getGripperList(GripperListBuilder gripperListBuilder,
Locale locale)
When the multi-gripper capability is registered (using the method
GripperCapabilities.registerMultiGripperCapability(GripperListProvider)), this method is called once (by
PolyScope) to retrieve the complete list of individual grippers/zones supported by this multi-gripper. |
GripperList getGripperList(GripperListBuilder gripperListBuilder, Locale locale)
GripperCapabilities.registerMultiGripperCapability(GripperListProvider)), this method is called once (by
PolyScope) to retrieve the complete list of individual grippers/zones supported by this multi-gripper.
Note This method is only called once, so it is not possible to add more grippers at a later time.
Grippers can, however, be created in an initial disabled state if needed. This can be useful, if
the gripper URCap is meant to support both a use case with only a single gripper as well as supporting the option
of mounting several separate, identical grippers on the robot at the same time (e.g. using on a special mounting
bracket). In this case, the secondary gripper(s) should still be added to the list, but can initially be disabled,
and then enabled (with MultiGripperCapability.setEnabled(SelectableGripper, boolean)) when the end user is
using a multi-gripper setup.
gripperListBuilder - A builder for creating individual grippers/zones and finally building the complete list
(to be returned by this method)locale - The current locale of PolyScope. Can be used for supporting gripper/zone names in several languages.nullLessThanTwoGrippers - if null is returned by this method (instead of a list)Copyright © 2024. All rights reserved.