@ProviderType
public interface ReleaseActionConfigBuilder
GripperNode instance.
Each configuration being built should ideally use a new ReleaseActionConfigBuilder instance. Note that if a
gripper selection was specified when the builder was used to create a configuration for a Gripper node (which is using
a multi-gripper device), then a new builder instance must be obtained to create a new configuration for another
Gripper node which is using a single gripper device.
GripperDevice.getCapabilitySupport(Class) to ensure that the gripper device used by a Gripper node
(accessible through GripperNode.getGripperDevice()) supports a specific capability (or set of capabilities)
before applying a configuration. Applying a configuration not supported by the gripper node/device will
throw an exception.| Modifier and Type | Method and Description |
|---|---|
ReleaseActionConfig |
build()
Build the gripper configuration for a Gripper program node
|
ReleaseActionConfigBuilder |
setEmptyGripperSelection()
Set an empty gripper selection for a Gripper node that uses a multi-gripper device, i.e.
|
ReleaseActionConfigBuilder |
setGripperSelection(Optional<SelectableGripper> gripperSelection)
Apply an existing gripper selection to a Gripper node that uses a multi-gripper device, i.e.
|
ReleaseActionConfigBuilder |
setGripperSelection(SelectableGripper gripper)
Select the specified individual gripper/zone for a Gripper node that uses a multi-gripper device, i.e.
|
ReleaseActionConfigBuilder setEmptyGripperSelection()
Set an empty gripper selection for a Gripper node that uses a multi-gripper device, i.e. a gripper device
supporting the multi-gripper capability (see the MultiGripperSupport interface). No individual gripper
will be selected in the Gripper node (any existing selection will be cleared).
GripperDevice.getCapabilitySupport(Class) with the class of the MultiGripperSupport interface as
argument to verify that the gripper device used by a Gripper node (accessible through
GripperNode.getGripperDevice()) supports multiple grippers. Attempting to apply a configuration to a
Gripper node (using GripperNode.setConfig(GripperNodeConfig)) will throw the UnsupportedConfig
exception, if the node uses a single gripper device.ReleaseActionConfigBuilder setGripperSelection(Optional<SelectableGripper> gripperSelection)
Apply an existing gripper selection to a Gripper node that uses a multi-gripper device, i.e. a gripper device
supporting the multi-gripper capability (see the MultiGripperSupport interface). The specified gripper/zone
selection must be taken from an existing configuration by using the return value of
GripActionConfig.getGripperSelection() or ReleaseActionConfig.getGripperSelection().
GripperDevice.getCapabilitySupport(Class) with the class of the MultiGripperSupport interface as
argument to verify that the gripper device used by a Gripper node (accessible through
GripperNode.getGripperDevice()) supports multiple grippers. Attempting to apply a configuration to a
Gripper node (using GripperNode.setConfig(GripperNodeConfig)) will throw the UnsupportedConfig
exception, if the node uses a single gripper device.gripperSelection - The existing gripper selection to apply, not nullReleaseActionConfigBuilder setGripperSelection(SelectableGripper gripper)
Select the specified individual gripper/zone for a Gripper node that uses a multi-gripper device, i.e. a gripper
device supporting the multi-gripper capability (see the MultiGripperSupport interface).
GripperDevice.getCapabilitySupport(Class) with the class of the MultiGripperSupport interface as
argument to verify that the gripper device used by a Gripper node (accessible through
GripperNode.getGripperDevice()) supports multiple grippers. Attempting to apply a configuration to a
Gripper node (using GripperNode.setConfig(GripperNodeConfig)) will throw the UnsupportedConfig
exception, if the node uses a single gripper device.gripper - The individual gripper/zone to be selected, not nullReleaseActionConfig build()
Copyright © 2021. All rights reserved.