Control panel with enabling device. Safety Case SaCa for retrofitting the UR control panel with a 3-postion enabling device to fulfil Robotic Safety standards. A robot pendant shall have a three-position enabling device to permit robot motion according to the robotic safety standard R15.06 and ISO 10218. The SaCa provide an "One hand use" of three-position enabling device and UR Freedrive button, so the second hand can be used for robotic guiding. The panel includes a protection cover for the UR teach panel. The original equipment from UR can be used without any changes. The Safety Case SaCa Control Panel is retrofitable of UR robots types: UR3, UR5, UR10 and reduces hazard for operators.