End Effectors Application

描述

The End Effectors application is used for configuring the tooling at the end of the arm, such as the tool center point (TCP) and center of gravity (CoG).

 

Using the End Effectors application functionality

  1. Go to the Application nodes screen. See “应用”选项卡.

  2. Tap the End Effectors icon.

    In the main screen, you can see End Effector application screen with a 3D robot view and an illustration of the Tool flange on the right panel. This change has been introduced to help users visualize the frame at the TCP and Tool Flange. On the left panel, the end effectors list now has the Robot group. The built-in Tool_flange end effector is located under that group.

 

Tool Center Point (TCP) wizards

The TCP wizards enables you to define the position and orientation of a TCP. The new wizards are accessible from the Tool Center Point application screen by tapping the new wizard icon next to the Position header and the Orientation header, respectively. In both wizards, you can call up a popup any time with more detailed instructions and animations on how to use the wizard. The instructions can be accessed by pressing the Instructions icon in the bottom left corner of the wizards.

 

  1. On the left panel, tap + Add End Effector.

  2. Tap TCP_1 under the newly added End_effector_1 tree.

  3. In the central panel, the Tool Center Point, you see the two wizard wand icons for Position and Orientation.

 

Adding, Renaming, Duplicating, and Deleting TCP

您可以通过以下操作开始配置新的 TCP:

  • Tap to define a new TCP with a unique name. The new payload appears in the End effector tree..

  • Tap to rename a TCP.

  • Tap to duplicate a TCP.

  • Tap to delete a selected TCP. 不能移除最后一个 TCP。

主动 TCP

The check-mark in the drop-down indicates which TCP is active .

默认的TCP

The default TCP is set as the active TCP before the program starts.

Select the desired TCP and tap to Set as default to set a TCP as the default.