Anwendungsvariablen

Beschreibung

Application Variables allows you to define a list of variables that are persisting between program runs and robot restarts. It can be used in the same way as any other variable(s) in the program. Along with values, variables can be exported together with program.

 

Using the Application Variables functionality

  1. Go to the application nodes screen. See Anwendung Tab.

  2. Tap the Application Variables icon.

     

     

  3. The Application Variables configuration page displays all created variables for the currently loaded program. Information is sorted in column by name, type, and value.

     

 

  1. On the screen’s top right side, tap the Create Variable button to add a new variable. A pop-up window appears with the name, type, and value fields for configuration.

     

     

  2. In the Name field, enter your variable name. Edit the value in the Value field. In the Type field, you see the allowed variable types and choose the one pertinent to your program.