Maintenance and Repair
| Safety for Maintenance |
The purpose of maintenance and repair is to ensure the system is kept functioning as expected. When working on the robot arm or control box, you must observe the procedures and warnings below. Failure to adhere to any of the safety practices, listed below, can result in injury.
|
| Safety for Maintenance |
Failure to leave space to accommodate the Control Box with the door fully open can lead to injury.
Disassembling the Control Box power supply too quickly after switching off, can result in injury due to electrical hazards.
After troubleshooting, maintenance, and repair work, ensure that safety requirements are fulfilled. Adhere to national or regional work safety regulations. The correct functioning of all safety function settings shall also be tested and validated.
|
| Lockout Tagout |
UR robots can be de-energized and locked in the de-energized state. This is to control hazardous energy due to tasks associated with installation, maintenance or repair of the robot, robot application or robot cell. To perform "Lockout" or "control of hazardous energy" of the power to the robot, you can use a power plug lock to prevent the power cord from being reattached to the Control Box, for example Brady 148081 Plug Lockout for IEC. Exposure to hazardous energy or the release of contained hazardous energy can result in electrical shock and serious injury.
|