Put in Box Predefined Position
| Description |
A predefined position has been added to the user interface in PolyScope 5. This replaces the previous put in box program. Put in box can be used to move the robot into a compact position that is suitable for transportation. The put in box sequence consists of an initial movement to the Zero Position, followed by a movement to the put in box position. |
| Put in Box |
This is how you find the predefined position:
The robot will now start the sequence. When the sequence is finished, the robot is ready to put in the official packaging.
|