EtherNet/IP

Description

EtherNet/IP is a network protocol that enables the connection of the robot to an industrial EtherNet/IP Scanner Device.

If the connection is enabled, you can select the action that occurs when a program loses EtherNet/IP Scanner Device connection.

Those actions are:

None
PolyScope ignores the loss of EtherNet/IP connection and the program continues to run.
Pause
PolyScope pauses the current program. The program resumes from where it stopped.
Stop

PolyScope stops the current program.