|
EtherNet/IP is a network protocol that enables the connection of the robot to an industrial EtherNet/IP Scanner Device.
If the connection is enabled, you can select the action that occurs when a program loses EtherNet/IP Scanner Device connection.
Those actions are:
|
None
|
PolyScope ignores the loss of EtherNet/IP connection and the program continues to run.
|
| Pause |
PolyScope pauses the current program. The program resumes from where it stopped. |
| Stop |
PolyScope stops the current program.
|
|