Adding External Equipment for Troubleshooting Purpose

For troubleshooting it can be useful to add a mouse, keyboard or monitor. Most USB mouse and keyboard types are supported. You can plug the mouse or keyboard in one of the available USB ports. A Control Box restart may required.

In the Control Box bracket, a Mini Display Port is available. When a monitor is connected, it displays the same content as the Teach Pendant. Both can be connected at the same time. It may be required to restart the Control Box for it to work.