Cleaning Your Robot

Everyday cleaning

You can wipe away any dust/dirt/oil observed on the robot arm and/or teach pendant using a cloth and one of the following cleaning agents:

  1. water

  2. 70% isopropyl alcohol

  3. 10% ethanol alcohol

  4. 10% naphtha

In rare cases, very small amounts of grease can be visible from the joint. This does not affect the function, use, or durability of the joint.

Additional cleaning

Due to the added focus on cleaning your robot, Universal Robots recommends cleaning with 70% isopropyl alcohol (rubbing alcohol).

  1. Wipe the robot with a hard twisted micro fiber cloth and 70% isopropyl alcohol (rubbing alcohol).
  2. Let the 70% isopropyl alcohol dwell on the robot for 5 minutes, and then clean the robot using standard cleaning procedure.

Do not use bleach Do not use bleach in any diluted cleaning solution.