Hardware Installation
| Description |
UR20 and UR30 robots have a built-it 3 Position Enabling functionality. e-Series robots do not have built-in 3 Position Enabling functionality. You can use the following instructions to replace a Teach Pendant and install a 3 Position Enabling Teach Pendant (3PE TP).
|
| Required items |
You need the following items to install the 3PE Teach Pendant:
|
| To remove a Teach Pendant |
Replacing the Teach Pendant can result in the system reporting a fault on start-up.
To remove the standard Teach Pendant:
|
| To install a 3PE Teach Pendant |
|