Electrical Installation: OEM AC FlexTail

Description

The main difference between the OEM Control Box and the OEM AC FlexTail is the cable extension between the Control Box and the robot arm connector, described in the following subsections.

 

The OEM AC FlexTail uses the same AC electrical installation described in the previous section. However additional items are required to attach the OEM AC FlexTail cable.

Installing or maintaining equipment connected to a power source can lead to electric shock.

  • Disconnect the equipment from the power source before installation or maintenance.
Required items

You need the following items to connect the wires:

  • The WAGO 831 four-pole female connector (included)
  • A flat-bladed screwdriver, blade 5.5 x 0.8 mm. For example: WAGO 210-721
  • Three wires with ferrule
  • Four M4 screws (not included)

 

The illustration below shows the required items.

 

1 Flat bladed tool 2 WAGO female connector (AC depicted)
3 Wire with ferrule    

How to Connect Wires to the Connector

Description

This section describes how to connect wires to a connector with locking levers:

To connect the wires
  1. Insert the screwdriver into a flat slot next to a connector hole.
  2. Push the screwdriver until the clamp inside the hole opens. Keep the screwdriver in the slot, as shown.

  3. Insert the wire ferrule into the open hole.
  4. Ensure that the wire ferrule is firmly placed, remove the screwdriver to close the hole.