Variable Waypoint
| Add a variable waypoint |
Add a variable waypoint that can be modified during run through of the robot program. |
| Add a variable waypoint to a robot program |
|
| Detail |
A waypoint with the position given by a variable, in this case calculated_pose.
The variable has to be a pose such as var=p[0.5,0.0,0.0,3.14,0.0,0.0].
The first three are x,y,z and the last three are the orientation given as a rotation vector given by the vector rx,ry,rz. The length of the axis is the angle to be rotated in radians, and the vector itself gives the axis about which to rotate. The position is always given in relation to a reference frame or coordinate system, defined by the selected feature.
If a blend radius is set on a fixed waypoint and the waypoints preceding and succeeding it are variable or if the blend radius is set on a variable waypoint, then the blend radius will not be checked for overlap (see Blending). If, when running the program, the blend radius overlaps a point, the robot will ignore it and move to the next one unless it is part of a smooth motion or OptiMove.
|