Assignment

Description

Assigns values to the variables. The variable value can be the result of expressions created in the Expression Editor (see section Expression Editor).

You can also request a variable value from an operator. When requesting a value from an operator, it is possible to display an Operator Message to validate input against common variable types.