Transportation
| Description |
Only transport the robot in its original packaging. Save the packaging material in a dry place if you want to move the robot later. When moving the robot from its packaging to the installation space, hold both tubes of the robot arm at the same time. Hold the robot in place until all mounting bolts are securely tightened at the base of the robot. Lift the Control Box by its handle.
|
|
Incorrect lifting techniques, or using improper lifting equipment, can lead to injury.
|
|
|
If the robot is attached to 3rd third-party application/ installation during transport, please refer to the following:
|
| Disclaimer |
Universal Robots cannot be held responsible for any damage caused by transportation of the equipment.
|
| Description |
Universal Robots always recommends transporting the robot in its original packaging. These recommendations are written to reduce unwanted vibrations in joints and brake systems and reduce joint rotation. If the robot is transported without its original packaging, then please refer to the following guidelines:
|
|
Transport |
|