I/O Interface Control
Description
|
The I/O Interface Control allows you to switch between user control and URcap control.
|
to use the I/O Interface Control |
If a URCap controls an end-effector, such as a gripper, then the URCap requires control of the Tool IO Interface. Select the URCap in the list, to allow it to control the Tool IO Interface.
|