Safety Message Types

Description

Safety messages are used to emphasize important information. Read all the messages to help ensure safety and to prevent injury to personnel and product damage.

Indicates a hazardous situation that, if not avoided, can result in death or serious injury.
Indicates a hazardous electrical situation that, if not avoided, can result in death or serious injury.
Indicates a hazardous hot surface where injury can result from contact and non-contact proximity.
 
Indicates a hazardous situation that, if not avoided, can result in injury.
Indicates grounding.
Indicates protective grounding.
 
Indicates the risk of damage to equipment and/or information to be noted.
Indicates more detailed information that should be consulted in the manual.