Verifying a successful calibration

The calibration is successful if the criteria listed below are met.

  • The mean deviation is less than 1 mm and 2 mrad.

  • The standard deviation is less than 0.5 mmand 1 mrad.

  • The difference between the Calibration Results and Control Results is no more than 50%.

  • In the Scale Result, the Error value is less than the Limit value.