Disassembly Screw Connection

Description
  1. Remove the screws in the blue lid, then remove the blue lid.

  2. Gently remove the power and communications wires from the terminals.

  3. You can use a small flathead screwdriver to push-off the flat-ring.

    Then slide the flat-ring over the joint.



  4. Remove Teflon-ring.

 
The joint can fall off if not supported when removing the screws.
  1. First remove the countersunk screws(a) then the remaining(b) screws.

  2. Note: Be very careful when removing the screws. Always use a correct sized, and undamaged screwdriver. The screw head slots can easily be stripped.

  3. The joint is now loose and can be removed. Remember to pull the wires out.