| bool |
A boolean variable whose value is either True or False. |
| int |
A whole number in the range from − 2147483648 to 2147483647 (32 bit). |
| float |
A floating point number (decimal) (32 bit). |
| string |
A sequence of characters.
|
| pose |
A vector describing the location and orientation in Cartesian space. It is a combination of a position vector (x, y, z) and a rotation vector (rx, ry, rz) representing the orientation, written p[x, y, z, rx, ry, rz].
|