Commissioning

Description

The following tests must be conducted before using the robot application for the first time or after making any modifications.

  • Verify all safety inputs and outputs are correctly connected.

  • Test all connected safety input and output, including devices common to multiple machines or robots, are functioning as intended.

  • Test emergency stop buttons and inputs to verify the robot stops and the brakes engage.

  • Test safeguard inputs to verify the robot motion stops. If safeguard reset is configured, check that it functions as intended.

  • Look at the initialization screen, activate the reduced input and verify the screen changes.

  • Change the operational mode to verify the mode icon changes in top right corner of PolyScope screen.

  • Test the 3-position enabling device to verify that pressing to the center on position enables motion in manual mode at a reduced speed.

  • If the Emergency Stop outputs are used, press the Emergency Stop push-button and verify that there is a stop of the whole system.

  • Test the system connected to Robot Moving output, Robot Not Stopping output, Reduced output, or Not Reduced output to verify the output changes are detected.

  • Determine the commissioning requirements of your robot application.