UR Connect
| Description |
The URCap UR Connect comes pre-installed with 5.19 PolyScope 5 software. To ensure correct operation, there are some additional prerequisites that must be installed. Please refer to the URCap documentation for additional information. UR Connect Installation and User Guide Go here for more information about the product: https://www.universal-robots.com/optimization-services/ur-connect/
|
| Install UR Connect |
To install the UR Connect, please follow the steps below:
|
| Activate UR Connect |
The UR Connect URCap needs to be paired with myUR to send data to MyUR. Please refer to the MyUR documentation on the UR Connect for further information.
|
| UR Connect URCap Update |
You can find the URCaps on the Installation Tab.
You can still update UR Connect even if it is NOT installed. |