Tool I/O
|
The tool connector illustrated below provides power and control signals for the grippers and sensors used on a specific robot tool. The tool connector has eight holes and is located next to the tool flange on Wrist 3. The eight wires inside the connector have different functions, as listed below:
The Tool Connector must be manually tightened up to a maximum of 0.4 Nm.
|
| Tool I/O Accessories |
The tool I/O for all Universal Robots robots can require an accessory element to facilitate connection with tools. You can use the Tool Cable Adapter.
|
| Tool Cable Adapter |
The Tool Cable Adapter is the electronic accessory that allows compatibility between tool I/O and tools.
Connecting the Tool Cable Adapter to a robot that is powered on can lead to injury.
The eight wires inside the Tool Cable Adapter have different functions, as listed below:
The tool flange is connected to GND (Ground).
|