Using the Robot without the IMM
| Description |
This section describes how to use an IMMI configured robot without the IMM. Disconnecting the IMM from the IMMI module triggers any Emergency Stops, rendering the robot unusable. A bypass plug closes the emergency and safety signals.
Use the bypass plug to allow the robot to function normally without being connected to the IMM.
The Control Box IP rating is maintained, when the bypass plug is connected. |
Connecting the Bypass Plug
| To connect the bypass plug |
|